Vishay Intertechnology's -30 V, 12 VGS P-Channel MOSFET Offers Industry’s Lowest RDS(ON) in its Class, Ratings Down to 2.5 V

2 mm by 2 mm PowerPAK® SC-70 Footprint Area Saves Space in Portable Electronics


SiA453EDJ

Products mentioned:

SiA453EDJ
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
MALVERN, Pa. — April 29, 2014 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new -30 V, 12 V VGS p-channel TrenchFET® power MOSFET in the ultra-compact, thermally enhanced PowerPAK® SC-70 package. With the industry's lowest on-resistance at -4.5 V and -2.5 V gate drives for a -30 V device in the 2 mm by 2 mm footprint area, the SiA453EDJ is designed to save space and increase power efficiency in portable electronics.

The -30 V VDS of the Vishay Siliconix device released today provides the headroom needed for over-voltage spikes, while its 12 V VGS enables lower on-resistance ratings of -3.7 V and -2.5 V for ultra-portable, battery-operated applications. The MOSFET is optimized for load and input over-voltage protection switches, battery chargers, and DC/DC converters in smartphones, tablet PCs, mobile computing devices, non-implantable portable healthcare products, hard disk drives, and handheld consumer electronics including electric toothbrushes, shavers, scanners, and RFID readers. For these applications, the SiA453EDJ offers extremely low on-resistance of 18.5 mΩ (-10 V), 23.5 mΩ (-4.5 V), 26.0 mΩ (-3.7 V), and 37.7 mΩ (-2.5 V), and provides built-in ESD protection of 4000 V.

The SiA453EDJ's on-resistance at -4.5 V is 36 % lower than the closest competing -30 V device, and 50 % lower than the closest competing device with a 12 V VGS. The MOSFET's on-resistance at -2.5 V is 46 % lower than the next-best 12 V VGS device. These industry-low values allow designers to achieve lower voltage drops in their circuits and promote more efficient use of power and longer battery run times, while the device's compact PowerPAK SC-70 package saves critical PCB space.

The MOSFET is 100 % Rg and UIS tested, halogen-free according to the JEDEC JS709A definition, and compliant to RoHS Directive 2011/65/EU.

Buy Now: To check distributor stock, please click here.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated