Vishay Intertechnology Launches New High-Voltage Thin Film Resistor Divider Network in Compact, Surface-Mount 1206 Case Size


Resistors
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
MALVERN, Pa. — Sept. 30, 2014 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new high-voltage thin film resistor divider network that offers a compact, higher-precision alternative to functionally equivalent products built on thick film technology.

The new Vishay Dale Electro-Films HVRD features an absolute tolerance to 1 %, ratio tolerance to 0.1 %, absolute TCR as low as 50 ppm/C, and TCR tracking of 10 ppm/C. Offered in a surface-mount 1206 format, the HVRD is compatible with high-speed assembly equipment, with edge castellation to allow visual inspection of solder joints.

Featuring a high 120 V maximum operating voltage, the HVRD will be used for voltage division in power converters, battery management circuitry, high-voltage test equipment, renewable energy and smart grid systems, and a wide range of industrial applications.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.