Vishay Intertechnology 500 mW Zener Diodes Save PCB Space With New Low-Profile MicroSMF eSMP® Series Package


Resistors

Products mentioned:

PLZ Series
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
MALVERN, Pa. — Nov. 5, 2014 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the first new series of Zener diodes with 500 mW of power dissipation in the new ultra-compact MicroSMF eSMP® series package. Combining extremely tight voltage tolerances with low leakage current and excellent stability, the PLZ-Series is designed to withstand ESD pulses of 8000 V (human body model), save PCB space, and increase pick-and-place speed for assembly lines.

The Vishay Semiconductors devices released today offer 500 mW power dissipation with voltage tolerances of ± 2.5 % in a symmetrical class SOD-323 flat lead package. With their compact footprints and low profiles of < 0.6 mm, PLZ-Series devices save significant PCB space when compared to diodes in similar plastic or glass SMD packages. The devices are optimized for voltage stabilization and reference voltage generation in power supplies and LED lighting.

PLZ-Series diodes feature a planar structure to guarantee high performance, ruggedness, and reliability characteristics. The devices provide a moisture sensitivity level (MSL) of 1 per J-STD-020, LF maximum peak of +260 °C; meet the JESD 201 Class 2 whisker test; and are RoHS-compliant, halogen-free, and Vishay GREEN. Ideal for automated placement, the diodes support wave and reflow soldering and allow for automated optical inspection (AOI) systems.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

eSMP is a registered trademark of Vishay Intertechnology