Vishay Intertechnology Wet Tantalum Capacitor Approved to DLA 15005, Offers Improved Vibration Capability, Thermal Shock, and Reverse Voltage for Avionics and Aerospace Systems


DLA 15005

Products mentioned:

DLA 15005
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
MALVERN, Pa. — March 24, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new tantalum-cased wet tantalum capacitor with a glass-to-tantalum hermetic seal that is approved to Defense Logistics Agency (DLA) drawing 15005. For avionics and aerospace systems, the device is the industry's first wet tantalum capacitor approved to DLA 15005 to combine a reverse voltage of 1.5 V at +85 C with improved vibration (sine: 50 g; random: 27.7 g) capability and thermal shock of 300 cycles.

Providing all the advantages of Vishay's SuperTan series devices — while offering improved reverse voltage for higher performance and enhanced vibration and thermal shock capabilities for increased reliability — the DLA 15005 electrolytic capacitor is optimized for timing, filtering, energy hold-up, and pulse power applications in power supplies for space and avionics equipment.

The device is initially offered in the axial T4 case size, with current voltage of 75 V, high capacitance of 1000 F, and capacitance tolerance of 10 % and 20 % standard at 120 Hz and + 25 C. The development of additional ratings and case sizes is underway. The DLA 15005 operates over a temperature range of -55 C to +85 C, to +125 C with voltage derating, and provides low maximum ESR of 0.50 Ω at 120 Hz and +25 C.

The capacitor released today features standard tin / lead (Pb) terminations, with RoHS-compliant 100 % tin terminations available.

Samples and production quantities of the DLA 15005 are available now, with lead times of 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

SuperTan is a registered trademark of Vishay Intertechnology