New Vishay Intertechnology BiSy Single- and Dual-Line, Low-Capacitance ESD Protection Diodes Save Board Space in Automotive Applications

Offered in Small SOT-323 Package, Devices Feature Capacitance Down to 10 pF for LIN-, CAN-, and FLEX-Bus Protection


VCAN26A2-03G VLIN26A1-03G VCAN26Diodes

Products mentioned:

VCAN26A2-03G
VLIN26A1-03G
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
MALVERN, Pa. — July 14, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today released new bidirectional symmetrical (BiSy) ESD protection diodes in the compact SOT-323 package. Measuring only 2.3 mm by 2.1 mm with a low 0.95 mm profile, the space-saving Vishay Semiconductors single-line VLIN26A1-03G and dual-line VCAN26A2-03G offer low capacitance and leakage current for the protection of automotive data lines against transient voltage signals.

For LIN bus applications, the VLIN26A1-03G provides transient protection for one data line as per IEC 61000−4−2 at 30 kV (air and contact discharge), while the VCAN26A2-03G protects two lines for CAN-Bus and FLEX-Bus applications. The AEC-Q101-qualified devices feature low load capacitance of 10 pF typical and 15 pF maximum, low maximum leakage current of < 0.05 A, and a working voltage of 26.5 V. The protection diodes are lead (Pb)-free and RoHS-compliant.

Samples and production quantities of the new VLIN26A1-03G and VCAN26A2-03G are available now, with lead times of eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.