Vishay Intertechnology to Highlight Industry-Leading Components at Solar Power International 2015


Solar Power
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — Sept. 1, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the Company will be highlighting its latest technologies and components at Solar Power International (SPI) 2015, being held Sept. 14-17 at the Anaheim Convention Center in Anaheim, California. Vishay’s technology line-up at the event will include a wide range of MOSFETs, diodes and rectifiers, optoelectronics, passive components, and custom magnetics optimized to meet the high demands of solar applications.

In booth 230 at SPI, Vishay will showcase a wide variety of the Company’s latest components. Highlighted resistors will include Vishay Dale Power Metal Strip® resistors with very high power ratings to 10 W, resistance values down to 0.0002 Ω and tight tolerances to ± 0.1 %. Also on display will be Vishay Dale precision thin film and thick film chip resistors with high power ratings to 22 W in case sizes from 0505 to 2512, Vishay Draloric high-voltage thick film resistors with voltage up to 500 V, and Vishay Techno thick film devices with wraparound or flip-chip terminations and voltages to 3 kV. Vishay Beyschlag high-voltage MELF resistors and Vishay high-voltage thin film chip resistors with voltage ratings to 1000 V will be on display for voltage detection, while Vishay Sfernice power resistors will be highlighted for discharge and snubber applications. Featured high-power grid resistors will include Vishay Milwaukee devices in IP00-, IP20-, and IP23-rated enclosures.

Film capacitors on display will include Vishay Roederstein metallized polypropylene film DC-link capacitors with capacitance up to 500 µF, snubber devices for direct IGBT and PCB mounting, and AC filtering capacitors, in addition to interference film devices offering high stability and humidity protection for X1, X2, and Y2 across-the-line applications. Highlighted inductors will include Vishay Dale low-profile, high-current IHLP® inductors and through-hole devices with high operating temperatures up to +180 °C and excellent DC/DC energy storage at frequencies to 2 MHz and greater.

At SPI, Vishay will also be showcasing custom magnetic solutions, such as resonant and full-bridge switchmode transformers with high power ratings to 7.5 kV, switching frequencies < 200 kHz, and low EMF. Featured custom magnetics will include inductors for filtering with inductance values to 1.5 mH and high current to 500 A, common-mode and differential-mode inductors featuring high power ratings to 1 MW and current to 1000 A, and three-phase grid tie inductors with inductance values to 700 µH and current to 500 A.

Vishay also offers a wide variety of semiconductor solutions for solar applications, including its E Series of high-voltage power MOSFETs built on superjunction technology for high-efficiency AC/DC power conversion in solar inverters, TMBS® Trench MOS Barrier Schottky rectifiers for photovoltaic solar cell bypass protection, FRED Pt® Gen 4 Ultrafast recovery diodes, opto-isolated IGBT / MOSFET drivers, high-speed 1 - and 10-MBd optocouplers in small-footprint SMD packages for compact inverters, and >1414 V high-isolation optocouplers in widebody packages featuring >10 mm creepage / clearance for industrial solar inverters and smart grid applications.

Produced by the Solar Energy Industries Association (SEIA) and the Solar Electric Power Association (SEPA), SPI is the largest solar trade show in North America. For more information, please visit http://www.solarpowerinternational.com/.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.