< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

New Vishay Intertechnology Bidirectional Single-Line ESD Protection Diodes in Small SOD-323 Package Save Board Space in Automotive Applications

For LIN Bus Protection, Devices Features Capacitance Down to 15.5 pF and Leakage Current of < 0.05 µA


Diodes

Products mentioned:

VLIN1626-02G
VLIN2626-02G
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — Jan. 6, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today released two new bidirectional single-line ESD protection diodes in the compact SOD-323 package. Measuring only 1.95 mm by 1.5 mm with a low 0.95 mm profile, the space-saving Vishay Semiconductors VLIN1626-02G and VLIN2626-02G offer low capacitance and leakage current for the protection of automotive data lines against transient voltage signals.

For LIN bus applications, the diodes released today provide transient protection for one data line as per IEC 61000-4-2 at ± 30 kV (air and contact discharge). The AEC-Q101-qualified devices feature low load capacitance of 15.5 pF typical and 18 pF maximum, low maximum leakage current of < 0.05 µA, and working voltages of -16 V / +26.5 V or ± 26 V. The protection diodes are lead (Pb)-free and RoHS-compliant.

Samples of the new VLIN1626-02G and VLIN2626-02G are available now. Production quantities are available now, with lead times of eight weeks for large orders.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: