For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology’s TVS Protection Diodes Safeguard Portable Electronics with 400 W Surge Capability in Compact SMF Package
The Industry’s First TVS to Feature a 2 % Breakdown Voltage Tolerance, Devices Offer Low 1 mm Profile, Low-Noise Technology, and Fast Response Times

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — Feb. 2, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new series of surface-mount transient voltage suppressor (TVS) protection diodes that are the industry’s first to feature a 2 % breakdown voltage tolerance. Offered in the low-profile SMF package, Vishay Semiconductors VTVSxxASMF series devices provide high surge capability of 400 W at 10/1000 µs for portable electronics.
With their low 1 mm profile, low-noise technology, and very fast response times, the devices released today are ideal for line transient voltage protection in space-constrained electronics, such as laptops, notebooks, tablets, smartphones, and external hard drives.
The VTVSxxASMF series consists of 23 devices with working voltages from 5 V to 63 V, with breakdown voltage tolerances of 2 % or 5 % available. The TVS offer a peak pulse current from 2.9 A to 20.3 A, excellent clamping capability from 14.8 V to 103.5 V, low incremental surge resistance, and operating temperatures from -55 °C to +175 °C.
The protection diodes provide ESD capability of ± 30 kV (air and contact discharge) in accordance with IEC 61000-4-2, support high-temperature soldering to 260 °C / 10 s at their terminals, and meet the MSL Level 1 standard per J-STD-020. The AEC-Q101-qualified devices are RoHS-compliant and halogen-free.
Samples and production quantities of the VTVSxxASMF series are available now, with lead times of eight weeks for larger orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: