< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Intertechnology vPolyTan Solid Tantalum Chip Capacitors Increase Volumetric Efficiency to Save Space in Handheld Consumer Electronics

Featuring MicroTan® Packaging Technology, Devices Offer Industry-Best Capacitance-Voltage Ratings in Six Molded Case Codes


T58

Products mentioned:

T58
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — Feb. 23, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of vPolyTan solid tantalum surface-mount chip capacitors that delivers increased volumetric efficiency for handheld consumer electronics. Combining polymer tantalum technology with Vishay’s high-efficiency MicroTan® packaging, the T58 series achieves industry-best capacitance-voltage ratings in six molded case codes, including 47µF-6.3V in the compact M0 (1608-10) case and 220µF-10V and 330µF-6.3V in the BB (3528-20).

Leveraging patented MAP (multi-array packaging) assembly technology, the capacitors released today provide a 10 % improvement in space utilization compared to similar devices, saving PCB space and enabling the design of smaller and thinner end products, including smartphones, tablets, and ultra-thin laptops, in addition to wireless cards, network equipment, and audio amplifiers and pre-amplifiers. In these devices, T58 series capacitors are intended for decoupling, smoothing, filtering, and energy storage applications.

The devices offer capacitance from 10 µF to 330 µF, with capacitance tolerance of ± 20 %, over voltage ratings from 4 V to 25 V in the MM (1608-09), M0 (1608-10), W9 (2012-09), A0 (3216-18), AA (3216-18), B0 (3528-10), and BB (3528-20) case codes. The capacitors feature low impedance, low ESR from 50 mΩ to 500 mΩ at 25 °C and 100 kHz, and ripple current from 0.224 A to 1.30 A at 100 kHz, and operate over a temperature range of -55 °C to +105 °C with voltage derating above +85 °C.

The rectangular molded case encapsulation of the T58 series is ideal for high-volume PCB assembly, and its special lead (Pb)-free L-shaped facedown terminations offer better contact to the solder pad than traditional facedown style terminations. RoHS-compliant, halogen-free, and Vishay Green, the devices feature a Moisture Sensitivity Level (MSL) of 3 and are available in tape and reel packaging per the EIA-481 standard.

Samples and production quantities of the T58 series capacitors are available now, with lead times of six to eight weeks for large orders.

Resources:

Polymer tantalum capacitors

Check distributor stock on the Vishay website

Weekly updates: sign up for Vishay Newsfeed

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: