For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology’s New 650 V Fast Body Diode MOSFETs Increase Voltage Headroom for Soft Switching in Industrial, Telecom, and Renewable Energy Applications

Products mentioned:
SiHA21N65EFSiHP21N65EF
SiHP28N65EF
SiHG28N65EF
SiHB21N65EF
SiHG21N65EF
SiHH21N65EF
SiHG33N65EF
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — May 5, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its portfolio of fast body diode n-channel power MOSFETs with the introduction of new 650 V EF Series devices. Augmenting the company’s 600 V offering, the Vishay Siliconix SiHx21N65EF, SiHx28N65EF, and SiHG33N65EF provide additional voltage headroom for industrial, telecom, and renewable energy applications when desired.
Built on E Series superjunction technology, the 650 V fast body diode MOSFETs released today feature a 10x lower reverse recovery charge (Qrr) than standard MOSFETs. This allows the devices to block the full breakdown voltage more quickly, helping to avoid failure from shoot-through and thermal overstress and increasing reliability in zero voltage switching (ZVS) / soft switching topologies such as phase-shifted bridges, LLC converters, and 3-level inverters.
The 21 A SiHx21N65EF is offered in five packages, while the 28 A SiHx28N65EF and 33 A SiHG33N65EF are each available in two. The devices feature low on-resistance down to 157 mΩ 102 mΩ and 95 mΩ respectively, and ultra-low gate charge. These values translate into extremely low conduction and switching losses to save energy in high-power, high-performance switch mode applications, including solar inverters, server and telecom power systems, ATX/Silver box PC SMPS, welding equipment, UPS, battery chargers, external electric vehicle (EV) charging stations, and LED, high-intensity discharge (HID), and fluorescent ballast lighting.
The devices are designed to withstand high energy pulses in the avalanche and commutation mode with guaranteed limits through 100 % UIS testing. The MOSFETs are RoHS-compliant and halogen-free.
Device Specification Table:
Part # | RDS(ON)(mΩ) @ 10 V (max.) |
Qg(nC) @ 10V (typ.) |
ID (A) @ 25 °C |
Qrr (µC)@ 25 °C (typ.) |
Package |
---|---|---|---|---|---|
SiHA21N65EF | 180 | 71 | 21 | 1.2 | Thin-lead TO-220 FullPAK |
SiHB21N65EF | 180 | 71 | 21 | 1.2 | D2PAK (TO-263) |
SiHG21N65EF | 180 | 71 | 21 | 1.2 | TO-247AC |
SiHH21N65EF | 157 | 68 | 21 | 0.9 | PowerPAK® 8x8 |
SiHP21N65EF | 180 | 71 | 21 | 1.2 | TO-220AB |
SiHG28N65EF | 102 | 97 | 28 | 1.1 | TO-247AC |
SiHP28N65EF | 102 | 97 | 28 | 1.1 | TO-220AB |
SiHG33N65EF | 95 | 114 | 33 | 1.18 | TO-247AC |
Samples and production quantities of the new 650 V EF Series MOSFETs are available now, with lead times of 16 to 18 weeks for large orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: