For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology Extends Voltage Range for Automotive Grade 146 CTI and 160 CLA Series SMD Aluminum Capacitors
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — May 17, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has extended the voltage range for its Automotive Grade 146 CTI and 160 CLA series of surface-mount aluminum capacitors to 100 V and 80 V, respectively. For high-temperature automotive and industrial applications, the Vishay BCcomponents devices provide low impedance, high ripple current, and long useful life.
146 CTI series capacitors are available in nine case sizes with operating temperatures to +125 °C, while the 160 CLA series is offered in six case sizes and provides high-temperature operation to +150 °C. The AEC-Q200-qualified devices feature low impedance down to 35 mΩ at 100 kHz for better filtering, a high rated ripple current to 1750 mA, and long useful life to 6000 h for high reliability.
For increased processing flexibility, the RoHS-compliant capacitors meet the rigorous JEDEC J-STD-020 soldering guidelines for severe reflow conditions. 146 CTI and 160 CLA series devices are charge- and discharge-proof, so there is no peak current limitation, and are offered in 4-pin and 6-pin versions for vibration-proof performance.
Polarized aluminum electrolytic capacitors with non-solid, self-healing electrolytes, the devices are ideally suited for smoothing, filtering, and buffering applications. Typical end products will include automotive power trains and chassis electronics; industrial drives, automation, and equipment for renewable energy; telecom equipment; and SMPS units.
Device Specification Table:
Series | 146 CTI | 160 CLA |
Ripple current at 100 kHz (mA) | 200 to 1750 | 270 to 1,400 |
Impedance at 100 kHz (mΩ) | 35 to 1,200 | 35 to 780 |
Capacitance range (µF) | 10 to 4,700 | 47 to 3,300 |
Tolerance (%) | ±20 | |
Voltage (V) | 16 to 100 | 16 to 80 |
Temp. range (°C) | -55 to +125 | -55 to +150 |
Useful life (h) | 6,000 | 2,000 |
Case sizes (mm) | 8 x 8 x 10 to 18 x 18 x 21 |
12.5 x 12.5 x 13 to 18 x 18 x 21 |
Samples and production quantities of the extended capacitors are available now, with lead times of six to 12 weeks for large orders.
Resources:
Automotive aluminum electrolytic capacitors
Check 80 V 146 CTI distributor stock on the Vishay website
Check 100 V 146 CTI distributor stock on the Vishay website
Check 80 V 160 CLA distributor stock on the Vishay website
Weekly updates: sign up for Vishay Newsfeed
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: