< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

New Vishay Intertechnology Conductive Aluminum Polymer Capacitors Provide Longer Useful Life, Higher Ripple Current, and Lower Impedance


180 CPS 181 CPL PolymerCapacitors

Products mentioned:

180 CPS
181 CPL
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — May 24, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced two new series of aluminum polymer capacitors featuring conductive technology. For portable electronics and consumer and telecom applications, Vishay BCcomponents 180 CPS and 181 CPL series devices provide higher ripple current, lower impedance, and longer useful life than standard aluminum capacitors.

Offered in a variety of case sizes from 5.3 mm by 5.3 mm by 5.7 mm to 10.4 mm by 10.4 mm by 12.6 mm, 180 CPS and 181 CPL series capacitors offer long useful life of 2500 h and 5000 h at +105 °C, respectively. The devices deliver ripple current to 6100 mA and impedance down to 9 mΩ.

The RoHS-compliant, surface-mount capacitors can support automatic placement and high-temperature reflow soldering according to JEDEC.

Device Specification Table:

Series 180 CPS 181 CPL
Rated ripple current at 100 kHz (mA) 2350 to 6100 900 to 5400
Impedance at 100 kHz (mΩ) 9 to 35 12 to 64
Useful life at +105 °C (h) 2,500 5,000
Case sizes (mm) 5.3 x 5.3 x 5.7 to
10.4 x 10.4 x 12.6
6.6 x 6.6 x 5.9 to
10.4 to 10.4 to 12.6
Capacitance range (µF) 22 to 2700 18 to 820
Tolerance (%) ±20
Voltage range (V) 2.5 to 35 4.0 to 35
Temperature range (°C) -55 to +105

Sample and production quantities of the 180 CPS and 181 CPL are available now, with lead times of 8 to 10 weeks for large orders.

Resources:

Aluminum electrolytic capacitors from Vishay

Check 180 CPS distributor stock on the Vishay website

Check 181 CPL distributor stock on the Vishay website

Weekly updates: sign up for Vishay Newsfeed

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: