For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology 1 W Axial Cemented, Fusible Wirewound Safety Resistor Offers Safe and Silent Fusing Operation
For Energy Meters, Home Appliances, and Power Supplies, Device Features Silent Fusing and Surge Voltage Capability of 2 kV

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — June 2, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 1 W axial cemented, fusible wirewound safety resistor that delivers safe and silent fusing operation during overload conditions, while withstanding pulse voltages of at least 2 kV (1.2 / 50 µs) per IEC 61000-4-5 for resistance values ≥ 75 Ω .
The Vishay Draloric AC01..CS combines a fusing time of < 30 s for a 32 W overload with a special non-flammable silicon cement coating for immediate interruption without flame and explosion when AC mains voltage (110 VAC / 230 VAC) is applied. Typical applications include electric appliances, energy meters, and power supplies.
The device released today is specially designed to meet UL1412 safety requirements (formal approval pending). In addition to fusing “without a bang,” the AC01..CS acts as an inrush current limiting resistor during normal operation. The safety resistor’s specially developed lacquer coating has superior thermal and electrical insulating properties. This allows designers to meet safety requirements more easily, while eliminating the need to put additional fuses in series with the input resistor.
The AC01..CS provides a power rating of 1.1 W at an ambient temperature of 40 °C and 1.0 W at 70 °C. The RoHS-compliant device offers resistance from 3 Ω to 100 Ω, resistance tolerance of ± 5 %, and temperature coefficient (TCR) of ± 200 ppm/K.
Samples and production quantities of the AC01..CS safety resistor are available now, with lead times of eight to 10 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
This release in:
- lang-code-EN
- lang-code-DE
- lang-code-JP
- lang-code-ZH