For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology CZB Series Thick Film Chip Attenuator With Balanced π Filter Saves Space, Simplifies Manufacturing
Device Replaces Three or More Discrete Components in Telecom and Mobile Wireless Products

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — June 14, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new surface-mount thick film chip attenuator featuring a balanced π filter schematic. Offered in a resistor array package, the Vishay Dale CZB can replace three or more discrete devices, reducing board space requirements and simplifying the manufacturing process in telecom and mobile wireless products.
As a single-component solution, the device released today delivers superior tolerance matching and temperature tracking for improved performance in signal attenuation applications. The CZB provides an attenuation range of 1.0 dB to 10.0 dB with an attenuation tolerance down to ± 0.3 dB.
The attenuator features maximum power dissipation of 0.075 W at +70 °C, a frequency range to 3 GHz, and impedance of 50 Ω and 75 Ω. The RoHS-compliant device operates over a temperature range of -55 °C to +150 °C.
Samples and production quantities of the CZB are available now, with lead times nominally of 8 to 10 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: