For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology Wireless Charging A11 Type Tx Coil for 5 V Applications Saves Space in Qi-Compatible Wireless Charging Pads
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — June 29, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new powdered-iron-based, WPC-compatible (Wireless Power Consortium) wireless charging A11 type transmitter coil for 5 V applications. AEC-Q200 qualification is pending. Offering a durable construction and high permeability shielding, the new Vishay Dale IWTX-47R0BE-11 6.3 µH is 18 % smaller than other solutions on the market to save space in Qi wireless charging pads, while providing high efficiency greater than 70 % when paired with a Vishay Rx coil and appropriate Qi-compatible Rx and Tx circuitry.
Designed for use in conjunction with Vishay’s WPC-compatible wireless receiver coils, the IWTX-47R0BE-11 6.3 µH’s high-saturation powdered iron is not affected by permanent locating magnets. As an alternative to larger ferrite-based solutions — which can saturate in the presence of a strong magnetic field — the IWTX-47R0BE-11 6.3 µH offers a magnetic saturation of 50 % at 4,000 gauss.
The RoHS-compliant device features low inductance of 6.3 µH at 200 kHz with a +5 % inductance tolerance, DCR of 38 mΩ (± 10 %) at + 25 °C, and Q of 190 typical at 200 kHz. The transmitter coil features a lead length of 47 mm and tinned length of 5 mm, and self-resonant frequency of 22 MHz.
Samples and production quantities of the IWTX-47R0BE-11 6.3 µH Tx coil are available now, with lead times of 14 weeks for large orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: