For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
New Vishay Intertechnology BiSy 2-Line, Ultra-Low-Capacitance ESD Protection Diode Saves Board Space in Portable Electronics
For Smartphones and Wearables, Compact Device Offers Low Profile < 0.4 mm and Capacitance Down to 0.35 pF Typical

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — July 11, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new bidirectional symmetrical (BiSy) 2-line ESD protection diode in the ultra-compact LLP1006-3L package for portable electronics. Saving space over solutions in the SOT23 package, the Vishay Semiconductors VBUS05M2-HT1 offers ultra-low capacitance and leakage current for the protection of high-speed data lines against transient voltage signals.
The device released today combines a low height of < 0.4 mm with low load capacitance of 0.35 pF typical. Featuring a “flow through” design, the VBUS05M2-HT1 is optimized for the protection of high-speed data lines including HDMI, DisplayPort, eSATA, USB 3.0, 1394 / FireWire, and Thunderbolt in smartphones, tablets, notebooks, and wearable devices. The protection diode features a low maximum leakage current of < 0.1 µA at the working voltage of 5.5 V, a breakdown voltage of 8.5 V typical at 1 mA, and a maximum clamping voltage of 18 V at 3.6 A.
The VBUS05M2-HT1 provides transient protection for data lines as per IEC 61000-4-2 at ± 20 kV (air and contact discharge). The device offers a moisture sensitivity level (MSL) of 1 in accordance to J-STD-020, a UL 94 V-0 flammability rating, and supports reflow soldering to +260 °C for 10 s. Soldering can be checked by a standard vision inspection, without the need for an x-ray. The protection diode is RoHS-compliant, halogen-free, and Vishay Green.
Samples and production quantities of the VBUS05M2-HT1 are available now, with lead times of eight weeks for large orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: