< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

New Vishay Intertechnology Series of Wide Terminal Thin Film Chip Resistors Features 1 W Power Rating in Compact 0612 Case Size

Lowering Costs, Devices Can Replace Multiple Resistors in Comparable Footprint or Larger Devices With Similar Power Ratings


For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — Sept. 8, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has extended its MCW AT Professional family of wide terminal thin film chip resistors by supplementing the existing MCW 0406 AT line with an additional case size for power handling of up to 1 W. For power electronics in industrial and automotive applications, Vishay Beyschlag MCW 0612 AT Professional devices provide high power dissipation, high-temperature performance, and renowned long-term thin film stability.

Offering up to four times higher power dissipation when compared to standard resistors in the 1206 footprint, the devices released today significantly lower costs by replacing multiple resistors of the same size or larger devices with equivalent power ratings. Furthermore, the wide terminal contact geometry of the MCW 0612 AT Professional series allows for superior robustness against thermal cycling. In addition, the resistors offer high operating temperatures to +175 °C for 1000 hours and advanced sulfur resistance as verified according to ASTM B 809 by exposure to sulfur vapor at 90 °C and 80 % to 90 % relative humidity for 42 days.

These specifications allow designers to use MCW 0612 AT Professional series resistors in harsh and high-temperature environments without compromising power rating or electrical performance, as well as to comply with today’s requirements for miniaturization. The devices are equally effective whether the application requires their full power capability or only a fraction of the nominal rated dissipation in order to gain improved stability. The resistors feature TCR down to ± 25 ppm/K, tolerance to ± 0.5 %, and a resistance range from 10 Ω to 100 kΩ

The MCW 0612 AT Professional series is the perfect choice for most fields of modern professional power electronics in which power dissipation, reliability, stability, and robust design are major concerns. Typical applications will include power measurement and control in lighting, inverters for hybrid electric vehicles (HEV) and electric vehicles (EV), engine control units, gear box controls, and braking and steering systems. For automotive applications, the resistors are qualified according to AEC-Q200.

Samples and production quantities of the MCW 0612 AT Professional series are available now, with lead times of eight to 10 weeks for large orders.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: