For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology WSKW0612 Power Metal Strip® Resistor Offers High Power and Low Resistance in 0612 Size to Save Space and Improve Efficiency
Featuring a Welded Terminal Construction and Kelvin 4-Terminal Connection, Device Increases Measurement Accuracy and Reduces TCR

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — Sept. 15, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new surface-mount Power Metal Strip® current sense resistor with an extended power rating of 1.0 W in the compact 0612 case size. For increased measurement accuracy, the Vishay Dale WSKW0612 features a welded copper terminal construction and a Kelvin 4-terminal connection that reduces TCR down to 75 ppm. The device offers low resistance values down to 0.001Ω to minimize excess power dissipation and improve end product efficiency.
Providing 4x the power of standard resistors in the 1206 footprint, the resistor released today allows designers to save board space and reduce costs by utilizing fewer and smaller components. The WSKW0612’s welded terminals reduce terminal resistance for higher accuracy than clad or electroplated terminals, while the low TCR provided by its 4-terminal connection reduces system measurement errors compared to typical 2-terminal devices.
The device’s advanced construction incorporates a solid metal nickel-chrome and manganese-copper resistive element with low TCR (< 20 ppm/°C). This results in a pulse-withstanding, tight-tolerance resistor that maintains the superior electrical characteristics of the Power Metal Strip construction. A proprietary processing technique produces extremely low resistance values ranging from 0.001 Ω to 0.003 Ω, with tolerances of ± 1.0 % and ± 5.0 %. The device provides low thermal EMF (< 3 µV/°C) and a temperature range from -65 °C to +170 °C.
The WSKW0612 is ideal for all types of current sensing and pulse applications in power management for cell phones; DC/DC converters for servers, VRMs for laptops, and Li-ion battery safety and management; industrial instrumentation and air conditioning inverters; and automotive electronic control such as engine, transmission, anti-lock brakes, audio, and climate controls. The device is RoHS-compliant, halogen-free, and Vishay Green.
For further information about the WSKW0612, Vishay’s application note “WSKW0612 Welded Terminal Advantage” provides an in-depth look at the benefits of the device’s terminals and Kelvin connection, outlines the differences between welded copper and copper-clad terminal construction, and provides a recommended pad layout.
Samples and production quantities of the new resistor are available now, with a lead time of six to eight weeks for larger orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: