For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology Low-Profile, High-Current Inductors Optimized for High-Frequency VRM10.0 Applications
Offered in 2727, 4027, 4031, and 5151 Case Sizes, Devices Offer Frequency Range to 2 MHz and Current to 71 A

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — Sept. 19, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of low-profile, high-current inductors for high-frequency VRM10.0 applications. Offered in the 2727,4027,4031, and 5151 case sizes, Vishay Dale IFLR series devices offer high saturation current to 71 A, very low DCR to 0.26 mΩ, and inductance down to 0.072 µH.
With a frequency range up to 2 MHz, the inductors released today serve as high-performing, space- and power-saving solutions for voltage regulator modules (VRMs) and DC/DC converters in notebooks, desktop computers, and servers; and low-profile, high-current power supplies and point of load (POL) converters.
Featuring a 100 % lead (Pb)-free shielded package, the RoHS-compliant devices are specified for an operating temperature range of -40 °C to +125 °C, with high resistance to thermal shock, moisture, mechanical shock, and vibration.
Device Specification Table:
Part # | IFLR-2727EZ-01 | IFLR-4027EZ-01 | IFLR-4031GC-01 | IFLR-5151HZ-01 |
---|---|---|---|---|
Case size | 2727 | 4027 | 4031 | 5151 |
Inductance (µH) | 0.072 to 0.150 | 0.085 to 0.220 | 0.170 to 0.215 | 0.21 to 0.44 |
DCR typ.(mΩ) | 0.32 | 0.38 | 0.26 | 0.32 |
DCR max. (mΩ) | 0.35 | 0.42 | 0.29 | 0.35 |
Heat rating current (A) | 45 | 50 | 61 | 50 |
Saturation current (A) | 30 to 58 | 33 to 70 | 44 to 60 | 35 A to 71 A |
Samples and production quantities of the IFLR series are available now, with lead times of 12 weeks for large orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
This release in:
- lang-code-EN
- lang-code-DE
- lang-code-JP
- lang-code-ZH