For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
New Vishay Intertechnology 4-Line ESD Protection Diode Provides Extreme Size Reduction for Portable Electronics
Featuring Ultra-Compact CLP1007-5L Package, Device Utilizes 70 % Less Board Space Than Previous-Generation Solutions

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — September 22, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 4-line ESD protection array for portable electronics in the ultra-compact chip-level CLP1007-5L package. Offering an extreme size reduction over previous-generation components without sacrificing performance, the Vishay Semiconductors VBUS54FD-SD1 offers low capacitance and leakage current for the protection of high-speed data lines against transient voltage signals.
Measuring only 1.0 mm by 0.7 mm with a low height of 0.27 mm, the protection array released today utilizes 70 % less board space than previous-generation devices and provides a seven-fold reduction in volume. Offering a low load capacitance of 0.9 pF typical and a “flow through” design, the VBUS54FD-SD1 is optimized for the protection of high-speed data lines including HDMI, DisplayPort, eSATA, USB 3.0, 1394 / FireWire, and Thunderbolt in mobiles phones, digital cameras, MP3 players, and portable gaming systems. The space-saving device also makes it possible to provide USB 3.0 interface protection in smartphones for the first time.
The protection array features a low maximum leakage current of < 0.1 µA at the working voltage of 5.5 V, a breakdown voltage of 7.5 V typical at 1 mA, and a maximum clamping voltage of 15 V at 3 A. The VBUS54FD-SD1 provides transient protection for data lines as per IEC 61000-4-2 at ± 15 kV (air and contact discharge). The device offers a moisture sensitivity level (MSL) of 1 in accordance to J-STD-020, supports reflow soldering to +260 °C for 10 s, and is Vishay Green.
Samples and production quantities of the new VBUS54FD-SD1 are available now, with lead times of eight weeks for large orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: