< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Intertechnology Ultra-Precision Thin Film Chip Resistor Delivers Extremely Low TCR of ± 2 ppm/°C and Tolerance of ± 0.01 % in Five Case Sizes


PLTU

Products mentioned:

PLTU
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — Oct. 31, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new ultra-precision thin film chip resistor that offers a dramatic improvement in TCR and tolerance over previous-generation devices. Available in five case sizes from 0603 to 2512, the Vishay Dale Thin Film PLTU offers a tight TCR of ± 2 ppm/°C and tolerance of ± 0.01 % for industrial, medical, military, and aerospace applications.

With stable film and performance characteristics of ± 0.04 % at +70 °C for 10,000 hours, the device released today is optimized for precision applications requiring low noise and high stability over time and temperature. End products will include test and measurement systems, instrumentation, weight scales, and military and avionics guidance systems.

The PLTU provides a wide resistance range from 100 Ω to 3 MΩ, with non-standard values available. The device offers very low noise of < -30 dB, a low voltage coefficient of 0.1 ppm/V, power dissipation ratings from 150 mW to 1 W, 75 V to 200 V maximum working voltages, and an operating temperature range of -55 °C to +125 °C.

The resistor features a high-purity alumina substrate and corrosion-resistant special passivation method (SPM) enhancement, and is available with lead (Pb)-free and lead (Pb)-bearing wraparound terminations over nickel barrier. The device is halogen-free and flame-resistant in accordance to UL 94 V-0.

Device Specification Table:

Case size Power rating (mW) Working voltage (V) Resistance range (Ω)
0603 150 75 100 to 130 k
0805 250 100 100 to 260 k
1206 400 200 100 to 775 k
2010 800 200 150 to 2 M
2512 1000 200 200 to 3 M

Samples and production quantities of the PLTU resistor are available now, with lead times of eight to 10 weeks.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: