For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
Vishay Intertechnology’s T58 Series of vPolyTan™ Polymer SMD Chip Capacitors Named 2016 EE Times and EDN ACE Award Finalist

Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — Nov. 17, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company’s T58 series of vPolyTan™ polymer surface-mount chip capacitors has been named a UBM 2016 EE Times and EDN ACE Award finalist in the Ultimate Products: Passives, Interconnects, and Electromechanical category. Designed to deliver increased volumetric efficiency for handheld consumer electronics, T58 series devices combine polymer tantalum technology with Vishay’s high-efficiency MicroTan™ packaging to achieve industry-best capacitance-voltage ratings in six molded case codes, including 47µF-6.3V in the compact M0 (1608-10) case and 220µF-10V and 330µF-6.3V in the BB (3528-20).
The EE Times and EDN ACE Awards showcase the best of the best in today’s electronics industry. Finalists for the Ultimate Products — awarded to the most significant electronic products introduced between January 1, 2015, and June 30, 2016 — were judged in 12 categories by a panel of EE Times and EDN editors, as well as industry experts. Final winners will be announced at the ACE Awards event, taking place on December 7 in San Jose, California, during Embedded Systems Conference (ESC) Silicon Valley.
Leveraging patented MAP (multi-array packaging) assembly technology, T58 series capacitors provide a 25 % improvement in space utilization compared with similar devices, saving PCB space and enabling the design of smaller and thinner end products, including smartphones, tablets, and ultra-thin laptops, in addition to wireless cards, network equipment, and audio amplifiers and pre-amplifiers. In these devices, T58 series capacitors are intended for decoupling, smoothing, filtering, and energy storage applications.
The devices offer capacitance from 10 µF to 330 µF, with capacitance tolerance of ± 20 %, over voltage ratings from 4 V to 25 V in the MM (1608-09), M0 (1608-10), W9 (2012-09), A0 (3216-18), AA (3216-18), B0 (3528-10), and BB (3528-20) case codes. The capacitors feature low impedance, low ESR from 50 mΩ to 500 mΩ at +25 °C and 100 kHz, and ripple current from 0.224 A to 1.30 A at 100 kHz, and they operate over a temperature range of -55 °C to +105 °C with voltage derating above +85 °C.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: