< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Intertechnology Bi-Directional 1500 W PAR® TVS Offer High Power Density to Save Board Space and Lower Costs

Surface-Mount Devices Feature eSMP® SMPC (TO-277A) Package With Low 1.1 mm Profile


TPCA11CA

Products mentioned:

TPC11CA thru TPC36CA
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — Nov. 21, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the industry’s first bi-directional 1500 W surface-mount PAR® transient voltage suppressors (TVS) in the low-profile eSMP® SMPC (TO-277A) package. With their low height of 1.1 mm typical, devices in the TPCxxCA series offer a 52 % lower profile than TVS in the traditional SMC package, while providing a 38 % smaller footprint to reduce total volume by 70 %. For designers, this high power density saves board space for lower system costs.

For high temperature stability in high-reliability conditions, the Vishay General Semiconductor TVS released today feature a patented PAR construction for a temperature range of −65 °C to +185 °C. The TPCxxCA series offers breakdown voltages from 11 V to 36 V, excellent clamping capability from 15.6 V to 49.9 V, low leakage current, and very fast response times.

The TVS components are designed to protect sensitive electronics against electrostatic discharge (ESD) and voltage transients induced by inductive load switching and lightning. Typical applications will include automotive, telecommunications, consumer electronics, and industrial equipment. Ideal for automated placement, the TVS meet MSL level 1 standards per J-STD-020, and are RoHS-compliant and halogen-free. The devices are available in AEC-Q101-qualified versions.

Samples and production quantities of the new TPCxxCA series are available now, with lead times of eight weeks for large orders.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: