< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Intertechnology vPolyTan Low-ESR Polymer Capacitors Increase Volumetric Efficiency to Lower Component Counts

Devices Offer Industry-Best Capacitance Density and Ultra-Low ESR in Molded EE (7343-43) Case Code


PolymerCapacitor

Products mentioned:

T59
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa. — Dec. 5, 2016 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of vPolyTan multi-anode polymer surface-mount chip capacitors that delivers increased volumetric efficiency for computing, telecom, and industrial applications. Combining polymer tantalum technology with Vishay’s patented multi-array packaging (MAP), the T59 series delivers the industry’s highest capacitance density, while maintaining best-in-class ESR.

Available in the molded EE (7343-43) case code, the capacitors released today offer up to 25 % better volumetric efficiency than similar devices, which allows for higher capacitance and voltage ratings. For example, their capacitance of 150 µF at 30 V is three times higher in capacitance than the closest competing device. In addition, the advanced packaging of the T59 series ensures ultra-low ESR from 25 mΩ to 150 mΩ at +25 °C and 100 kHz.

The devices offer capacitance from 15 µF to 470 µF, with capacitance tolerance of ± 20 %, over voltage ratings up to 75 V. By replacing multiple lower-capacitance devices, T59 series capacitors reduce component counts to save PCB space and lower costs in solid-state drives, networking equipment, and motherboards. In these products, the capacitors are intended for decoupling, smoothing, filtering, and energy storage applications.

The T59 series features ripple current from 1.3 A to 3.1 A at 100 kHz, and an operating temperature range of -55 °C to +105 °C. RoHS-compliant, halogen-free, and Vishay Green, the devices offer both lead (Pb)-free and tin/lead (Sn/Pb) wraparound terminations, and are available in tape-and-reel packaging per the EIA-481 standard. The capacitors are 100 % surge current tested to ensure robust performance in high-inrush-current applications.

Samples and production quantities of the T59 series are available now, with lead times of 10 weeks for large orders.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in: