For more information:
Media contact -
Bob Decker, Red Pines Group
Phone:
1.415.409.0233
Fax:
1.650.618.1512
E-mail:
bob.decker@redpinesgroup.com
Sales contact:
New Vishay Intertechnology Wireless Charging Coils Offer Direct Replacements for EOL Devices
Rx and Tx Coils Deliver High Efficiency for Portable Electronics, Qi Wireless Charging Pads
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact:
MALVERN, Pa. — Apr. 29, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced new powdered iron based, WPC-compliant (Wireless Power Consortium) wireless charging coils that offer direct replacements for devices for which end-of-life (EOL) was announced in 2017. Offering a durable construction and high permeability shielding, the Vishay Dale receiver and transmitter coils provide high efficiency in a variety of industry-standard sizes.
For wireless charging up to 10 W in portable electronics, the six new receiver coils feature inductance of 10.8 µH to 22 µH at 200 kHz with ± 5 % inductance tolerance, typical Q from 29 to 65 at 200 kHz, and DCR from 175 mΩ to 427 mΩ (± 5 %) at +25 °C.
For Qi wireless charging pads, the three new transmitters offer inductance of 6.3 µH to 24 µH at 200 kHz with a ± 5 % inductance tolerance, DCR from 40 mΩ to 75 mΩ (± 5 %) at + 25 °C, and typical Q from 185 to 200 at 200 kHz. The devices are available with heat rated current of 6 A and 7 A, and saturation current of 20 A and 22 A.
Device Compatibility Table:
Original part number |
Replacement part number |
IWAS3222BZEB190J50 |
|
IWAS3827ECEB100J50 |
|
IWAS4832FFEB9R7J50 |
|
IWAS4832FEEB150J50 |
|
IWAS4832ECEB220J50 |
|
IWTX4646BEEB240J50 |
|
IWTX47R0BEEB6R3J11 |
|
IWTX47R0BEEB240K11 |
Samples and production quantities of the wireless charging coils are available now, with lead times of 12 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that
are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace,
and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
Media contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales contact: