Products mentioned:
NSR HPMedia Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Jan. 24, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of wirewound noise suppressor resistors that delivers improved voltage performance and reliability for automotive ignition systems in reciprocating engines.
Vishay Dale NSR-HP series devices feature a coating that increases reliability by protecting the resistive element against moisture and mechanical shock, while enabling high voltage performance to 45 kV and high operating temperatures to +200 °C. The resistors can withstand high voltage pulses at high frequencies and feature a dielectric withstand voltage of 1000 VAC.
Ideal for reducing RFI during electrical discharges in gasoline engines, the NSR-HP series can be used in spark plug leads, as well as in spark plug caps. The devices are available with wide ohmic and inductance value ranges from 1 kΩ to 15 kΩ and 9 µH to 78 µH, respectively, and feature a temperature coefficient of ± 250 ppm/°C.
The resistors are RoHS-compliant, halogen-free, and Vishay Green.
Samples of the NSR-HP series are available now. Production quantities will be available in March, with lead times of 16 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/