Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Apr. 10, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company will be exhibiting its latest grid and ribwound resistors for oil and gas, industrial, traction, and renewable energy power systems at the 2018 IEEE PES T&D Conference and Expo, the largest and most comprehensive show in the transmission and distribution industry. Taking place April 16-19 at the Colorado Convention Center in Denver, Vishay will be highlighting the Vishay Milwaukee GRE1, GRE2, and GRE3 series of high power, high current grid resistors, RBEF / RBSF series of ribwound resistors, and NGR series of neutral ground resistors in booth 2236.
Vishay’s GRE1, GRE2, and GRE3 series grid resistors are optimized for capacitor pre-charge and discharge, dynamic braking, load testing, heater, and neutral grounding applications in locomotive, harmonic filters, and renewable energy and industrial systems. The devices offer high power ratings to 36 kW at +40 °C, high operating temperatures to +415 °C, a wide resistance range from 0.02 Ω to 240 Ω — with tolerance of ± 10 % — and low inductance from 5 µH to 150 µH. Featuring double insulation for maximum cooling efficiency, the resistors can be mounted in IP00, IP20, and IP23 enclosures for indoor and outdoor use.
Ideal for pulsing applications, RBEF / RBSF series ribwound resistors are designed to meet heavy-duty requirements in systems where space is at a premium. Providing high reliability, the devices offer an all-welded construction and are available with high temperature silicone or vitreous enamel coatings. The resistors feature power ratings from 40 W to 2 kW, a wide on-resistance range from 0.010 Ω to 525 Ω, and are available individually with simple hardware, open mounted on bracket, or mounted inside screened or outdoor-rated enclosures.
NGR series devices offer high temperature performance to +760 °C in rugged, weatherproof IP23-rated enclosures. Designed to provide ground fault, overvoltage, and short circuit protection for generators and transformers in wye (star) configurations without exceeding the temperature limitations outlined by IEEE-32, the resistors deliver extremely high line-neutral voltage to 8 kV, system voltage to 13.8 kV, and current ratings to 1,000 A. The devices offer a tied live design to eliminate floating voltages in the assembly.
More information on the 2018 IEEE PES T&D Conference and Expo is available at http://www.ieeet-d.org/IEEE18/public/enter.aspx.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/