Vishay Intertechnology 225 EDLC-R ENYCAPTM Series Honored With 2018 AspenCore World Electronics Achievement Award
225 EDLC-R ENYCAPTM Series Wins the High Performance Passive Component Category

Products mentioned:
VCNL4030X01Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Nov. 20, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company’s ruggedized 225 EDLC-R ENYCAPTM series of electrical double-layer energy storage capacitors has received a 2018 AspenCore World Electronics Achievement Award. For energy harvesting and power backup applications in harsh, high humidity environments, the devices are the industry’s first to offer useful life of 2000 hours at +85 °C and meet the highest class of moisture resistance: the biased 85 / 85 1000-hour test.
Presented by AspenCore, the world’s largest media group within the technical electronics sector, the World Electronics Achievement Awards (WEAA) program honors companies and individuals who have made outstanding contributions to innovations and development in the electronics industry worldwide. Product award winners are selected through online voting by engineers around the globe. This year, Vishay’s 225 EDLC-R ENYCAPTM series received the most votes in the High Performance Passive Component category.
The long useful life of 225 EDLC-R ENYCAPTM series capacitors is double that of standard EDLCs, while their high moisture resistance allows them to be used in applications where high humidity would compromise standard devices. This allows for maintenance-free operation to lower costs, while providing engineers with greater design flexibility in a wide range of industrial, renewable energy, and automotive applications.
Available in eight small case sizes ranging from 16 mm by 20 mm to 18 mm by 40 mm, 225 EDLC-R ENYCAPTM capacitors offer high power density to 4.1 Wh/kg, capacitance values from 20 F to 60 F, and a maximum rated voltage of 2.7 V. The RoHS-compliant devices feature rapid charge and discharge performance and are available in through-hole versions.
Award winners were recognized at a ceremony held during the Global CEO Summit in Shenzhen, China. Gerald Tatschl, Senior Manager, Product Marketing, Aluminum, was on hand to accept the award on Vishay’s behalf.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
ENYCAP is a trademark of Vishay Intertechnology