Vishay Intertechnology Launches New Ruggedized ENYCAP™ Energy Storage Capacitors for Long Life and High Moisture Resistance
For Harsh, High Humidity Environments, 225 EDLC Double-Layer Capacitors Feature Useful Life of 2000 Hours, Biased 85 / 85 1000-Hour Testing

Products mentioned:
259 PHM-SIMedia Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — May 10, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of ruggedized ENYCAP™ electrical double-layer energy storage capacitors for energy harvesting and power backup applications in harsh, high humidity environments. Vishay BCcomponents 225 EDLC-R ENYCAP capacitors are the industry’s first to offer useful life of 2000 hours at +85 °C and meet the highest class of moisture resistance: the biased 85 / 85 1000-hour test.
The long useful life of the devices released today is double that of standard electrical double-layer capacitors, enabling maintenance-free operation and greater design flexibility. Their high humidity resistivity allows for use in a wide range of industrial, renewable energy, and automotive applications, including smart meters, handheld electronics, robotics, solar panels, E-latch door systems, and emergency lighting.
Available in eight small case sizes ranging from 16 mm by 20 mm to 18 mm by 40 mm, 225 EDLC-R ENYCAP capacitors offer high power density to 4.1 Wh/kg, capacitance values from 20 F to 60 F, and a maximum rated voltage of 2.7 V. The RoHS-compliant devices feature rapid charge and discharge performance and are available in through-hole versions.
Samples and production quantities of the 225 ELDC-R ENYCAP capacitors are available now, with lead times of six weeks for larger quantities.
Resources:
ENYCAP energy storage capacitors from Vishay
Check distributor stock on the Vishay website
Weekly updates: sign up for Vishay Newsfeed
ENYCAP is a trademark of Vishay Intertechnology.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/