Vishay Intertechnology Snap-in Power Aluminum Capacitors Save Space, Lower Costs for Power Supplies, Solar Inverters, and Motor Controls
Devices Offer Increased Ripple Current to 4.42 A and Useful Life of 3000 Hours at 105 °C

Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — May 16, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of miniature snap-in power aluminum electrolytic capacitors. Ideal for power supplies, solar inverters, and industrial motor controls, the Vishay BCcomponents 259 PHM-SI series combines 30 % higher ripple current than previous-generation components with a long useful life.
With ripple currents up to 4.42 A, the devices released today allow designers to utilize fewer components to save board space and lower costs. Their long useful life of 3000 hours at 105 °C permits demanding applications requiring more than 10 years of lifetime from capacitors in ambient temperatures to 60 °C.
Featuring a cylindrical aluminum case, insulated with a blue sleeve, 259 PHM-SI series devices feature rated voltages to 500 V in 25 compact case sizes ranging from 22 mm by 25 mm to 35 mm by 60 mm. The RoHS-compliant capacitors are also available with 3-pin keyed polarity snap-in terminals.
As polarized aluminum electrolytic capacitors with a non-solid electrolyte, the devices are ideally suited for buffering, filtering, and energy storage in compact power applications, including power supplies for server farms or industrial tools such as plasma cutters; motor drives for compressors in industrial cooling systems; and industrial lamp drivers for UV water treatment systems.
Device Specification Table:
Case size (D x L in mm) | 22 x 25 to 35 x 60 |
Capacitance range | 39 µF to 2200 µF |
Tolerance | ± 20 % |
Ripple current at 100 Hz and +105 °C | 0.53 A to 4.42 A |
Rated voltage | 200 V to 500 V |
Category temperature range | -40 °C to +105 °C |
Useful life at +105 °C | 3000 h |
Max. ESR at 100 Hz | 80 mΩ to 3.31 Ω |
Max. impedance at 10 kHz | 60 mΩ to 2.44 Ω |
Sectional specification | IEC 60384-4/EN130300 |
Climatic category IEC 60068 | 40/105/56 |
Samples and production quantities of the 259 PHM-SI series capacitors are available now, with lead times of 15 weeks.
Resources:
Aluminum electrolytic capacitors from Vishay
Check distributor stock on the Vishay website
Weekly updates: sign up for Vishay Newsfeed
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/