Vishay Intertechnology to Highlight Leading Military-Qualified and COTS Resistors and Tantalum Capacitors at CMSE 2018
Vishay Products for Avionics Aerospace, Military, and Commercial Space Systems

Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — May 1, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company will be showcasing its extensive offering of military-qualified and COTS resistors and tantalum capacitors at the 2018 Components for Military and Space Electronics (CMSE) conference and exhibition. The event will take place May 7-10 at the Sheraton Four Points Hotel in Los Angeles.
Now in its 22nd year, CMSE is the premier event focused on the design, reliability, and application of electronic components for use in avionics aerospace, military, and commercial space systems. At the conference, Vishay Dale will be displaying a wide range of military-qualified resistors with established reliability. These will include leaded through-hole metal film resistors; thick and thin film chip resistors; leaded and housed wirewound devices; and thick and thin film resistor networks.
Featured military-qualified tantalum capacitors at CMSE 2018 will include through-hole, surface-mount, and high energy wet tantalum capacitors; Vishay Sprague conformal-coated and molded tantalum chip capacitors with a wide range of capacitance / voltage ratings; and surface-mount polymer capacitors that undergo high reliability processing, including surge current testing, accelerated aging, thermal cycling, and hot DLC screening. In addition, Vishay Sprague will highlight Hi-Rel COTS solid surface-mount tantalum capacitors with MIL screening and voltages to 75 V.
At CMSE 2018, Vishay will also be highlighting a wide range of high precision resistors for non-QPL military applications. Featured products will include Vishay Huntington and Vishay Milwaukee ribwound and roundwire power resistors with power ratings to 2000 W and resistance values down to 0.01 Ω; Vishay Dale Power Metal StripÃ’ resistors with low resistance values down to 0.0001 Ω, high stability metal film resistors with tolerances to ± 0.01 %, flameproof metal film resistors with power ratings to 3 W in compact sizes, and thick film resistors with high power ratings to 22 W; Vishay Techno high and medium voltage thick film chips and dividers; and Vishay Dale Thin Film resistors and networks for high temperature operation up to +250 °C.
More information about CMSE 2018 is available at https://www.tjgreenllc.com/cmse/.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com
Sales Contact: http://www.vishay.com/
en/company/contacts/