Vishay Intertechnology Receives 2018 Design & Elektronik Innovator of the Year Award
Company Recognized for Development of the HOTcap® K…H Series of Automotive Grade MLCCs
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
MALVERN, Pa. — Dec. 12, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has been honored by Design & Elektronik magazine with a 2018 Innovator of the Year Award in recognition of its development of the HOTcap® K…H series of Automotive Grade, radial-leaded multilayer ceramic chip capacitors (MLCCs).
The Innovator of the Year Awards recognize the stars behind the products for the top technologies they have developed. Finalists in ten categories were selected by Design & Elektronik editors, while winners were determined by online voting. This year, Vishay received the most votes in the “Passive Components” category for its K…H series.
K…H series MLCCs are approved for operation over a temperature range of -55 °C to +200 °C for 500 hours, and they provide unlimited operation to +175 °C. The devices combine their high temperature performance with a wide capacitance range from 100 pF to 1 μF and low capacitance tolerances as tight as ± 5 %. The Ceramic Class 1 MLCCs feature an ultra stable C0G dielectric with a capacitance change of ± 30 ppm/K whereas the Class 2 MLCCs feature a X0U dielectric with TCC of +22 % / -56 % from -55 °C to +175 °C.
Ideal for EMI filtering in sensors and DC motors in the most extreme automotive environments, HOTcap® K…H series capacitors are equipped with a high reliability MLCC insert produced in a unique wet build process and featuring noble metal electrodes. AEC-Q200 qualified with PPAP available on request, the leaded MLCCs are more robust to mechanical and thermal stress and can withstand higher operating temperatures than SMD parts.
The 2018 Innovator of the Year Awards were presented in a ceremony in Munich. Markus Roessler, Product Marketing, Ceramic Capacitors, accepted the award on Vishay’s behalf.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
HOTcap is a registered trademark of Vishay Intertechnology