Vishay Intertechnology AEC-Q200 Qualified, 150 W Thick Film Power Resistor in Clip Mount TO247 Reduces Component Counts, Costs

Designed for Direct Mounting on a Heatsink, Device Offers Industry-High Power Dissipation and Improved Pulse Handling Capability

LTO150
For more information:
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in:

MALVERN, Pa.July 30, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new AEC-Q200 qualified thick film power resistor featuring a clip mount TO247 package for direct mounting on a heatsink. For automotive applications, the Vishay Sfernice LTO 150 offers industry-high power dissipation of 150 W at a +45 °C case temperature and an improved pulse handling capability.

The device released today provides up to 70 % higher power dissipation than competing devices in the TO247 package. This reduces the need for components to cool the resistor — saving board space, simplifying layouts, and reducing overall solution costs. These benefits are amplified by the LTO 150’s 30 % improvement in energy handling compared to similar TO247 devices, which allows designers to utilize fewer resistors.

Offering high temperature operation to +175 °C and a broad range of resistance values from 0.03 Ω to 1.3 MΩ, the LTO 150 serves as the precharge or discharge resistor for inverters, converters, and on-board chargers for electric vehicles (EV), hybrid electric vehicles (HEV), and plugged hybrid electric vehicles (PHEV). It can also be used in general industrial and military power conversion applications. The RoHS-compliant device offers a non-inductive design, tolerances down to ± 1 %, and superior reliability tests results (i.e. extensive temperature cycling from 1000 cycles and up).

Samples and production quantities of the new resistor are available now, with lead times of 8 to 12 weeks. 

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

twitter http://twitter.com/vishayindust
facebook http://www.facebook.com/VishayIntertechnology

###

For more information:
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in: