Vishay Intertechnology Introduces Industry’s First IHLP® Inductor Series Qualified to MIL-STD-981 Class S for Space-Grade Applications

SGIHLP Devices Feature High Operating Temperatures to +180 °C in a Rugged Package

SGIHLP
For more information:
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in:

MALVERN, Pa.April 25, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduces a new series of low profile, high current IHLP® inductors that are the industry’s first to meet the requirements of MIL-STD-981 class S. Designed to provide high reliability in space-grade applications, inductors in the Vishay Custom Magnetics SGIHLP series feature a ruggedized package and perform at high operating temperatures to +180 °C.

Featuring a magnetically shielded construction, the devices released today are optimized for DC/DC converters and high current noise suppression filters in satellites and defense systems. Applications for the inductors include low profile, high current power supplies and point of load (POL) converters; “flight-ready” solar inverters; high current filters; and DC/DC converters in distributed power systems.

Offered in five case sizes, the SGIHLP series features high efficiency with typical DCR from 0.56 mW to 240 mW and a wide range of inductance values from 0.22 µH to 100 µH. Based on proven IHLP technology, the devices provide rated currents to 100 A and handle high transient current spikes without saturation. The inductors offer excellent inductance and saturation stability over the complete operating temperature range.

Device Specification Table:

Part number

SGIHLP-24DC-8

SGIHLP-48FA-8

SGIHLP-60HE-8

SGIHLP-73HF-8

SGIHLP-97OZ-8

Case size

24DC

48FA

60HE

73HF

97OZ

Dimensions (mm)

6.2 x 6.7

x 4.3

12.2 x 12.9

 x 6.1

15.5 x 15.2

x 8.5

18.8 x 19.2 x 8.6

27.2 x 24.5

x 15.0

Inductance (µH)

0.22 to 15

0.47 to 68

0.22 to 22

0.47 to 47.0

0.47 to 100

DCR typ. (mW)

3.95 to 195

1.55 to 240

0.73 to 31.30

0.89 to 52.7

0.56 to 36.25

DCR max. (mW)

4.23 to 208

1.66 to 252

0.81 to 33.49

0.95 to 56.4

0.67 to 39.40

Heat rating current (A)

2.4 to 18

2.4 to 30

8.3 to 66

7.25 to 65.0

9.1 to 80

Saturation current (A)

1.6 to 11

3.5 to 28.5

5.5 to 68

7.0 to 76.0

7.0 to 100

SRF typ. (MHz)

14.1 to 190

4.02 to 72.1

6.43 to 113

3.72 to 52.3

2.01 to 47.5

For more information about the new inductors and to place orders, contact CustomMags@Vishay.com. Technical datasheets can be found at www.Vishay.com by entering SGIHLP in the “Part # / Keyword Search” field.

IHLP is a registered trademark of Vishay Intertechnology

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

twitter http://twitter.com/vishayindust
facebook http://www.facebook.com/VishayIntertechnology

###

For more information:
Media Contact - Paul Harrison, Senior MarCom Manager
Phone: +49 9287 712 808
Fax: +49 9287 712 809
E-mail: paul.harrison@vishay.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in: