Vishay Intertechnology High Speed PIN Photodiode Offers Enhanced Sensitivity for Visible Light, Enables Slim Sensor Designs for Wearables
Device Delivers Precise Signal Detection in 4.8 mm by 2.5 mm SMD Package With Industry-Low 0.48 mm Profile
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
MALVERN, Pa. — May 21, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today broadens its optoelectronics portfolio with the introduction of a new high speed silicon PIN photodiode with enhanced sensitivity for visible light. Featuring a rectangular 4.8 mm by 2.5 mm top-view, surface-mount package with an industry-low 0.48 mm profile — 0.37 mm lower than competing solutions — the Vishay Semiconductors VEMD8080 offers fast switching times and low capacitance of 47 pF for precise signal detection in wearable devices and medical applications.
With a radiant-sensitive area measuring 4.5 mm² — and high radiant sensitivity with a reverse light current of 28 µA and dark current of 0.2 nA — the device released today utilizes Vishay’s proven wafer technology to detect visible and near infrared radiation over a wide spectrum range from 350 nm to 1100 nm. For green LEDs, the VEMD8080’s sensitivity represents a 30 % improvement over the standard technology in previous-generation solutions.
When used with green LEDs, such as Vishay’s VLMTG1400, the photodiode’s small size and high sensitivity enable slim sensor designs for optical heart rate detection in wearable devices such as fitness trackers and smart watches. In these devices, the VEMD8080’s rectangular shape allows several light emitting diodes to be placed close to the radiant sensitive area to maximize the signal. When combined with 660 nm and 940 nm dual color emitting diodes, the photodiode is ideal for SpO2 measurement in medical monitors.
The VEMD8080 features a ± 65° angle of half-sensitivity, temperature range of -40 °C to +85 °C, and 950 nm wavelength of peak sensitivity. RoHS-compliant, halogen-free, and Vishay Green, the photodiode provides a moisture sensitivity level (MSL) of 4 in accordance with J-STD-020 for a floor life of 72 hours.
Samples of the VEMD8080 are available now. Production quantities will be available in March 2018, with lead times of eight to 10 weeks for large orders. A product demo board is available from MikroElektronika and Vishay distributors.
For the latest in all things opto — articles, videos, and products — visit Vishay's Opto Squad blog site: www.vishayopto.com.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.