Vishay Intertechnology Can Now Add Heart Rate Monitoring Capability to Any Type of Consumer Electronics Device
Prototype Fitness Watch to Showcase Capability at electronica 2018

Products mentioned:
TFBR4650Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Nov. 7, 2018 — The Optoelectronics group of Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it can help manufacturers add a heart rate monitoring capability to any type of consumer electronic device. Vishay will demonstrate the capability at electronica 2018 with a fitness watch prototype that uses Vishay optoelectronic components to enable the heart rate monitor function in conjunction with a software algorithm developed by Elfi-Tech Ltd., a developer of unique non-invasive medical devices.
With this capability, Vishay is creating an opportunity for companies that don’t have proprietary software and hardware solutions for heart rate monitoring to add the capability to their products with a relatively low cost of entry. Together Vishay and Elfi-Tech can supply a complete reference design for the heart rate monitoring capability, including digital and analog front end components.
Enabling Vishay optoelectronic components in the fitness watch on view at electronica 2018 include the VEMD5080X01 PIN photodiode and VLMTG1400 LED. The VEMD5080X01 is a unique surface-mount device that eliminates optical cross-talk. It is sensitive to visible and infrared light from 350 nm to 1100 nm and comes in a tiny package measuring 7.5 mm by 7.5 mm by 0.9 mm. The VLMTG1400 LED has a peak wavelength in the green spectrum at 525 nm and features typical intensity of 1400 millicandela. It is packaged in a 0603 surface-mount format with height of 0.55 mm.
Elfi-Tech provided the software and the non-optical hardware of the fitness watch including an Arm® Cortex®-M3 microcontroller, a Texas Instruments analog front-end for heart-rate monitoring, Bluetooth Low Energy connectivity, and MEMS based accelerometer. Output is transmitted to an Android application.
The fitness watch will be demonstrated in booth C4.422 at electronica 2018 taking place Nov. 13-16 at the Munich Trade Fair Centre in Munich. For more information on the heart monitoring capability and reference design, contact sensorstechsupport@vishay.com. More on Vishay at electronica is available at http://www.vishay.com/landingpage/tradeshows/electronica2018/.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
Elfi-Tech, Ltd. is a leader in the field of non-invasive measurement of physiological parameters, using proprietary optical sensors and algorithms. The company has developed and is constantly improving on its range of novel personal health monitoring, patient monitoring, and home monitoring products. Elfi-Tech is unique in its ability to conduct continuous and non-invasive monitoring of numerous physiological parameters. Learn more about Elfi-Tech’s suite and international strategic partnerships at www.Elfi-Tech.com.