Vishay Intertechnology’s High Speed IR Emitters Named as 2019 Elektra Awards Finalists
VSMY5850X01, VSMY5890X01, and VSMY5940X01 Shortlisted in “Semiconductor Product of the Year — Analog” Category
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
This release in:
- English
- 简体中文
MALVERN, Pa. — Nov. 26, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its Vishay Semiconductors VSMY5850X01, VSMY5890X01, and VSMY5940X01 high speed infrared (IR) emitters have been selected as finalists for the 2019 Elektra Awards in the category of “Semiconductor Product of the Year — Analog.”
Presented by Electronics Weekly magazine, the Elektra Awards recognize individuals and companies for their excellent performance, innovation, and contributions to the global electronics industry, with winners selected in 22 categories by an independent panel of expert judges. Finalists in the “Semiconductor Production of the Year — Analog” category were chosen based on demonstrated technical capabilities that differentiate them from competing products.
Traditional IR emitter PCB packages utilize an all-transparent epoxy to embed the emitter chip, resulting in side emissions that can cause a halo effect in camera images. The 2 mm by 1.25 mm by 0.8 mm 0805 surface-mount package of Vishay’s VSMY5850X01 (850 nm), VSMY5890X01 (890 nm), and VSMY5940X01 (940 nm) features opaque side walls, which prevent unwanted side emissions. This provides a distinct advantage for position tracking in virtual or augmented reality applications. Furthermore, the opaque side walls simplify designs by eliminating the need for external barriers such as rubber rings.
With Vishay’s SurfLightTM surface emitter chip technology, the IR emitters deliver 30 % higher radiant intensity than previous-generation devices over a wide temperature range from -40 °C to +110 °C. The devices are qualified according to AEC-Q101, making them suitable for automotive applications such as the emitters in rain sensor modules. They also outperform standard IR emitters in proximity sensors, optical switches, and miniature light barriers. While standard devices emit light in all directions, the SurfLight VSMY5850X01, VSMY5890X01, and VSMY5940X01 emit nearly all of their light and power out of the top of the chip. With most of the light concentrated on the surface, the IR emitters achieve higher intensity to 13 mW/sr.
Award winners will be announced at the Elektra Awards Dinner, taking place in London on Dec. 4 at the Grosvenor House, Park Lane.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
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
This release in:
- English
- 简体中文