Vishay Intertechnology 3 V Ruggedized ENYCAP™ Energy Storage Capacitors Offer Long Life and High Moisture Resistance
For Harsh, High Humidity Environments, 235 EDLC Double-Layer Capacitors Feature Useful Life of 2000 Hours, Biased 85 °C / 85 % RH1500-Hour Testing

Products mentioned:
235 EDLC-HVR ENYCAP™Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Oct. 21, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of 3.0 V ruggedized ENYCAP™ electrical double-layer energy storage capacitors for energy harvesting and power backup applications in harsh, high humidity environments. Vishay BCcomponents 235 EDLC-HVR ENYCAP capacitors are the industry’s first such high voltage devices to offer useful life of 2000 hours at +85 °C and meet the highest class of moisture resistance: the biased 85 °C / 85 % RH 1500-hour test.
The long useful life of the devices released today is double that of standard electrical double-layer capacitors, enabling maintenance-free operation and greater design flexibility. Their high humidity resistivity allows for use in a wide range of industrial, renewable energy, and automotive applications, including smart meters, handheld electronics, robotics, solar panels, E-latch door systems, and emergency lighting.
Available in 15 small case sizes ranging from 10 mm by 20 mm to 18 mm by 40 mm, 235 EDLC-HVR ENYCAP capacitors offer high power density and capacitance values from 5 F to 60 F. The RoHS-compliant devices feature rapid charge and discharge performance and are available in through-hole versions.
Samples and production quantities of the 235 EDLC-HVR ENYCAP capacitors are available now, with lead times of six weeks for larger quantities.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
ENYCAP is a trademark of Vishay Intertechnology