Vishay Intertechnology’s IHSR-1616AB-01 Tapped as Electronics Industry Awards 2019 Finalist
High Saturation Commercial Inductor Delivers Low DCR, High Current Density for Multi-Phase Power Supplies
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
MALVERN, Pa. — May 28, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its IHSR-1616AB-01 high saturation commercial inductor has been named as an Electronics Industry Awards 2019 finalist in the “Power Product of the Year” category.
Organized by Datateam Business Media — the publisher of CIE magazine — the Electronics Industry Awards recognize outstanding people, products, and business practices in the electronics sector. Five finalists and one winner in each category were determined through a combination of voting by industry professionals and scoring by an expert panel of judges. Vishay’s IHSR-1616AB-01 impressed both with its 50 % reduction in DCR over typical power inductors and standard DCR tolerance of 5 %, with 3 % tolerance available for more accurate current sensing.
Offered in the compact 4 mm by 4 mm 1616 case size with a low 1.2 mm profile, the IHSR-1616AB-01’s low typical DCR down to 1.15 mΩ and inductance up to 0.068 µH allow for higher current density than competing technologies. As a result, the device can replace larger single-turn ferrite inductors to save space, enable slimmer end products, and deliver better temperature stability for multi-phase, high current power supplies and filters in computer, industrial, and telecom applications
With a frequency range up to 5 MHz, the IHSR-1616AB-01 is optimized for energy storage in DC/DC converters and high current filtering up to the self-resonant frequency (SRF) of the inductor (418 MHz to 856 MHz). The device offers high temperature operation to +125 °C, rated current to 62 A, and handles high transient current spikes without saturation.
Winners of the Electronics Industry Awards 2019 will be announced on Friday, June 21, during a ceremony held at The Tower Hotel in London.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.