Vishay Intertechnology Common-Drain Dual N-Channel 60 V MOSFET Increases Power Density and Efficiency

For Bidirectional Switching in 24 V Systems, Device Features Best in Class RS‑S(ON) Down to 10 mΩ Typical and Industry-Low RS-S(ON) per Area

SiSF20DN

Products mentioned:

SiSF20DN
For more information:
Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in:

MALVERN, Pa.Dec. 11, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new common-drain dual n-channel 60 V MOSFET in the compact, thermally enhanced PowerPAK® 1212-8SCD package. Designed to increase power density and efficiency in battery management systems, plug-in and wireless chargers, DC/DC converters, and power supplies, the Vishay Siliconix SiSF20DN offers the industry’s lowest RS-S(ON) in a 60 V common-drain device.

The dual MOSFET released today provides RS-S(ON) down to 10 mΩ typical at 10 V, the lowest among 60 V devices in the 3 mm by 3 mm footprint. This value also represents a 42.5 % improvement over the next best solution in this footprint size and is 89 % lower than Vishay’s previous-generation devices. The result is reduced voltage drops across the power path and minimized power losses for increased efficiency. For higher power density, the SiSF20DN’s RS1S2(ON) times area is 46.6 % lower than the next best alternative MOSFET, even when including larger 6 mm by 5 mm solutions.

To save PCB space, reduce component counts, and simplify designs, the device uses an optimized package construction with two monolithically integrated TrenchFET® Gen IV n‑channel MOSFETs in a common drain configuration. The SiSF20DN’s source contacts are placed side by side, with enlarged connections increasing the contact area with the PCB and reducing resistivity further compared to conventional dual package types. This design makes the MOSFET ideal for bidirectional switching in 24 V systems and industrial applications, including factory automation, power tools, drones, motor drives, white goods, robotics, security/surveillance, and smoke alarms.

The SiSF20DN is 100 % Rg- and UIS-tested, RoHS-compliant, and halogen-free.

Samples and production quantities of the new MOSFET are available now, with lead times of 30 weeks for larger orders.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

twitter http://twitter.com/vishayindust
facebook http://www.facebook.com/VishayIntertechnology

###

PowerPAK is a registered trademark of Siliconix incorporated

 

For more information:
Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in: