Vishay Intertechnology T55 Series of Polymer Tantalum Chip Capacitors Now Available in Z Case (EIA 7343-19) Size
With Lower Profile Than Standard V Case, Devices Increase Package Density and Enable Design of Thinner End Products

Products mentioned:
T55Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Feb. 6, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has extended its T55 series of vPolyTan™ surface-mount polymer tantalum molded chip capacitors with new devices in the Z case (EIA 7343-19) size.
With a 0.1 mm lower height than devices in the standard V case (EIA 7343-20), the Vishay Polytech capacitors released today increase package density and enable the design of thinner end products. The devices are optimized for power management, battery decoupling, and energy storage in computers, servers, network infrastructure equipment, solid-state drives, and wireless transceivers.
Offered in the compact J, P, A, B, T (low-profile B — 1.2 mm max), D, V, and Z case sizes, the T55 series features a wide capacitance range from 3.3 µF to 680 µF, over voltage ratings from 2.5 V to 63 V, and a capacitance tolerance of ± 20 %. The capacitors provide ultra low ESR from 500 mΩ down to 7 mΩ at +25 °C, a result of their polymer cathodes, which offer greatly enhanced performance over manganese dioxide devices. Capacitance values up to 1000 µF and ESR values down to 6 mW are in development.
Operating over a temperature range of -55 °C to +105 °C, the capacitors offer excellent ripple current rating up to 5.66 A IRMS and provide low internal resistance for enhanced charge and discharge characteristics. Featuring lead (Pb)-free terminations, the T55 series is RoHS-compliant, halogen-free, and Vishay Green. The devices are compatible with high volume automatic pick and place equipment and offer a Moisture Sensitivity Level (MSL) of 3.
Samples and production quantities of the T55 series capacitors in the Z case size are available now, with lead times of 12 to 14 weeks.
Resources:
More tantalum capacitors from Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
vPolyTan is a trademark of Vishay Intertechnology