Vishay Intertechnology Extends T55 Series of Polymer Tantalum Chip Capacitors With Single-Digit ESR Down to 7 mΩ in the D Case
Devices Feature Reduced Voltage Drops, Better Frequency Response, and Higher Ripple Currents Ratings Up to 5.67 A IRMS

Products mentioned:
T55Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — June 5, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has extended its T55 series of vPolyTan™ surface-mount polymer tantalum molded chip capacitors with new devices in the D case (EIA 7343-31) size featuring single-digit ESR values from 9 mΩ down to 7 mΩ, with values to 6 mΩ in development.
Previously reserved for larger case sizes, the single-digit ESR values of the capacitors released today are 3 mΩ to 5 mΩ lower than those typically found in D case devices. The result is reduced voltage drops, better frequency response, and higher ripple current ratings up to 5.67 A IRMS, which reduces the number of capacitors required on the PCB. In addition to saving board space, the D case’s low 3.1 mm profile enables the design of thinner end products.
Offered in the compact J, P, A, B, T (low-profile B — 1.2 mm max), D, V, and Z case sizes, the T55 series features a wide capacitance range from 3.3 µF to 1000 µF over voltage ratings from 2.5 V to 63 V, and a capacitance tolerance of ± 20 %. The devices are optimized for power management, battery decoupling, and energy storage in computers, servers, network infrastructure equipment, solid state drives, and wireless transceivers.
Operating over a temperature range of -55 °C to +105 °C, the capacitors provide low internal resistance for enhanced charge and discharge characteristics. Featuring lead (Pb)-free terminations, the T55 series is RoHS-compliant, halogen-free, and Vishay Green. The devices are compatible with high volume automatic pick and place equipment and offer a Moisture Sensitivity Level (MSL) of 3.
Samples and production quantities of the new single-digit ESR capacitors are available now, with lead times of 14 to 16 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology
###
vPolyTan is a trademark of Vishay Intertechnology