New Vishay Intertechnology 2.5 A IGBT and MOSFET Driver Delivers Increased Efficiency for Inverter Stages
Device Features High Peak Output Current of 2.5 A for Motor Drives, Alternative Energy, and Other High Voltage Applications

Products mentioned:
VOD3120AB, VOD3120AD, VOD3120AGMedia Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Feb. 4, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today broadened its optoelectronics portfolio with the introduction of a new 2.5 A IGBT and MOSFET driver. Available in DIP-8 and SMD-8 packages, the Vishay Semiconductors VOD3120A features low voltage drop on its output at a low current consumption of 3.5 mA to increase efficiency in inverter stages
Built on CMOS technology, the optocoupler released today consists of an AIGaAs LED optically coupled to an integrated circuit with a rail to rail output stage, which provides the drive voltages required by gate-controlled devices. The voltage and current supplied by the VOD3120 make it ideal for directly driving IGBTs with ratings up to 1200 V / 100 A.
With high isolation voltage ratings of VIORM = 891 V and VIOTM = 6000 V, the device provides galvanic isolation for motor drives, solar inverters, switchmode power supplies (SMPS), induction stovetops, and uninterruptable power supplies (UPS). In addition, its undervoltage lock-out (UVLO) feature protects IGBTs / MOSFETs from malfunction, while its common mode transient immunity of 35 kV/μs minimum helps to reduce noise issues from high to low voltage areas on the PCB.
The optocoupler offers a maximum propagation delay time of 0.5 µs for applications requiring fast switching. The RoHS-compliant device operates over a wide power supply range of 15 V to 30 V and an industrial temperature range from -40 °C to +105 °C.
Samples and production quantities of the VOD3120 are available now, with lead times of six weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.