Vishay Intertechnology to Showcase Latest Power Management Solutions for Next-Generation Applications at PCIM Europe 2023

Company to Highlight Industry-Leading Technologies in a Series of Demonstrations Focused on E-Mobility and Energy Storage

Vishay Intertechnology to Showcase Latest Power Management Solutions for Next-Generation A
For more information:
Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in:

MALVERN, Pa.May 4, 2023 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that at PCIM Europe 2023, the company will be showcasing its broad portfolio of power management solutions that address two increasingly important trends in power electronics: e-mobility and energy storage. In Hall 9, Booth 210, Vishay experts will be available to discuss the company’s extensive offering of passive and semiconductor solutions for these next-generation applications, including the development of 600 V and 1200 V planar SiC MOSFET technology; power inductors that enable high efficiency in gallium-nitride (GaN) DC/DC converters; and integrated power module solutions that combine high efficiency fast body diode MOSFETs and SiC, FRED Pt®, and MOAT diode technologies to enable higher power density than discrete solutions.

Vishay will also be offering a variety of product-focused demonstrations at PCIM. Visitors to the company’s booth with see ENYCAP™ electrical double-layer energy storage capacitors being used in batteryless mobile applications, while optocoupler evaluation boards will highlight the functionality of the VOA300 linear optocoupler for voltage and current sensing; VOM1271 photovoltaic MOSFET driver with integrated fast turn-off; and VOW2611 widebody high speed optocoupler.

Application-focused demonstrations will also include:

  • A 40 kW resettable electronic fuse (eFuse) for 400 V and 800 V battery electric vehicles (BEV)
  • A unidirectional, 11 kW three-phase AC on-board charger (OBC) with a BOM consisting of 90 % Vishay parts
  • A high voltage intelligent battery shunt for 400 V and 800 V batteries
  • A bidirectional 10 kW eFuse for 48 V applications
  • A V-harvester board featuring an e-peas controller and Vishay photodiodes and hybrid energy storage capacitors
  • A collaborative robot workstation featuring Vishay power resistors, ESTA power electronic capacitors (PEC), and Automotive Grade diodes

Additional Vishay passive components on display at PCIM will include haptic feedback actuators; Power Metal Strip® and Power Metal Plate™ resistors; ultra precision thin film chip resistors and fuses; power thick film resistors; knob potentiometers; metallized polypropylene film capacitors; ceramic AC and DC disc capacitors; and radial, snap-in, and surface-mount aluminum electrolytic capacitors. Highlighted Vishay semiconductor solutions will consist of 2 A to 7 A TMBS® rectifiers up to 150 V, 2 A to 4 A standard rectifiers up to 600 V, and 1 A to 5 A 200 V FRED Pt ultrafast rectifiers in Vishay’s first compact, low profile Power DFN series package: the industry-first DFN3820A. In addition, 600 V and 1200 V FRED Pt Gen 5 and Gen 7 ultrafast and hyperfast rectifiers in a variety of power packages will be on display, as well as 400 V, 600 V, and 1200 V standard rectifiers in eSMP® series SlimDPAK 2L and SMPD 2L packages.

PCIM Europe 2023 — an exhibition for power electronics, intelligent motion, renewable energy, and energy management — will be taking place May 9-11 at the Messe Nuremberg, Germany. More information on the event is available at https://pcim.mesago.com/nuernberg/en.html.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

twitter https://twitter.com/vishayindust
facebook https://www.facebook.com/VishayIntertechnology

###

The DNA of tech™ is a trademark of Vishay Intertechnology.

For more information:
Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com

Sales Contact: http://www.vishay.com/
en/company/contacts/

This release in: