News » 2020 Releases » Vishay Intertechnology Automotive Grade DC-Link Film Capacitors Deliver S ...

Vishay Intertechnology Automotive Grade DC-Link Film Capacitors Deliver Stable Capacitance and ESR in High Humidity Environments

AEC-Q200 Qualified Metallized Polypropylene Devices Withstand THB Testing

MKP1848HDC-Link

Products mentioned:

MKP1848H DC-Link
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
MALVERN, Pa. — Sep. 9, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of Automotive Grade DC-Link metallized polypropylene film capacitors optimized for high humidity environments. The Vishay Roederstein MKP1848H DC-Link is Vishay’s first series of AEC-Q200 qualified DC-Link film capacitors to withstand temperature humidity bias (THB) testing — 85 °C, 85 %  relative humidity for 1000 hours at rated voltage — without altering its electrical characteristics.

The radial capacitors released today are designed to ensure extremely stable capacitance and ESR values over a long service life under harsh environmental conditions during operation. The robust devices are ideal for output filtering in automotive on- and off-board chargers and DC/DC converters; power converters for solar farms; auxiliary power supplies in wind energy generators; industrial power supplies and motor drives; welding equipment; and UPS.

MKP1848H DC-Link series capacitors offer rated capacitance from 1 µF to 80 µF and low ESR down to 3 mΩ. The devices provide high ripple current capabilities up to 25.1 A and rated voltages of 500 VDC, 700 VDC, 800 VDC, 920 VDC, and 1200 VDC at +85 °C. The capacitors are RoHS-compliant, halogen-free, and Vishay Green.

Samples of the MKP1848H DC-Linkseries are available now. Production quantities will be available in Q3 2020 with a lead time of 20 weeks.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
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
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.®


Contact Us |
Where to Buy
  • Find a Distributor
  • Find a Sales Representative
| Request Sample | Technical Support | Privacy Center | Do Not Sell or Share My Personal Information | Terms and Conditions | Information Security | Terms of Use |

CONNECT WITH US

Copyright ©2025 Vishay Intertechnology, Inc.

ECIA Member