Vishay Intertechnology 200 V N-Channel MOSFET in PowerPAK® 1212‑8S Offers Industry-Low RDS(ON) to Increase Power Density, Save Energy
TrenchFET® Device Offers Typical RDS(ON) of 61 mΩ and FOM of 854 mΩ*nC in 10.89 mm² Package

Products mentioned:
SiSS94DNMedia Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Sep. 23, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 200 V n-channel MOSFET that offers industry-low typical on-resistance of 61 mΩ at 10 V in the 3.3 mm by 3.3 mm thermally enhanced PowerPAK® 1212-8S package, in addition to improved on-resistance times gate charge — a critical figure of merit (FOM) for MOSFETs used in switching applications — of 854 mΩ*nC. Purpose-built to increase power density, the space-saving Vishay Siliconix SiSS94DN is 65 % smaller than devices with similar on-resistance in 6 mm by 5 mm packages.
The typical on-resistance of the TrenchFET® Gen IV power MOSFET released today is 20 % lower than the next best product on the market in a similar package size, and its FOM is 17 % lower than the previous-generation solution. These values result in reduced conduction and switching losses to save energy. With its compact size, the flexible device allows designers to save PCB space by replacing a much larger MOSFET with the same conduction losses, or a similar sized MOSFET with higher conduction losses.
The SiSS94DN is ideal for primary-side switching for isolated DC/DC topologies and synchronous rectification in telecom equipment, computer peripherals, and consumer electronics; LED backlighting for notebooks, LED TVs, vehicles, and vessels; and motor drive control, load switching, and power conversion for GPS, factory automation, and industrial applications.
The device is 100 % RG- and UIS-tested, RoHS-compliant, and halogen-free.
Samples and production quantities of the SiSS94DN are available now, with lead times of 12 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
 https://www.facebook.com/VishayIntertechnology
 https://www.facebook.com/VishayIntertechnology
###
The DNA of tech™ is a trademark of Vishay Intertechnology.
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/