New Vishay Intertechnology TMBS® Rectifiers in Low Profile SMP Package Increase Power Density and Efficiency
2 A and 3 A Devices Feature Reverse Voltages From 45 V to 200 V and Forward Voltage Drop Down to 0.36 V

Products mentioned:
Selector GuideMedia Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Jan. 22, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its offering of surface-mount TMBS® Trench MOS Barrier Schottky rectifiers with 16 new 2 A and 3 A devices in the eSMP® series low profile SMP (DO-220AA) package. The Vishay General Semiconductor rectifiers feature a wide range of reverse voltages from 45 V to 200 V, while their 3 A rating is the industry’s highest for the SMP package to increase power density.
With their forward voltage drop down to 0.36 V for 2 A and 0.37 V for 3 A devices, the rectifiers released today reduce power loss and improve efficiency in high frequency inverters, DC/DC converters, and freewheeling and polarity protection diodes for commercial and industrial applications. The devices are also available in AEC-Q101 qualified versions for automotive applications.
The new rectifiers feature a maximum operating junction temperature up to +175 °C and an MSL moisture sensitivity level of 1, per J-STD-020, LF maximum peak of +260 °C. The devices are RoHS-compliant and halogen-free.
Device Specification Table:
Part # | IF(AV) (A) | VRRM (V) | IFSM (A) | VF at IF and TJ | TJ max. (°C) | ||
VF (V) | IF (A) | TA (°C) | |||||
V2PL45L | 2 | 45 | 50 | 0.36 | 2 | 125 | 150 |
V3PL45 | 3 | 45 | 80 | 0.37 | 3 | 125 | 150 |
V2P6X | 2 | 60 | 50 | 0.51 | 2 | 125 | 175 |
V2P6L | 2 | 60 | 50 | 0.45 | 2 | 125 | 150 |
V2PM6L | 2 | 60 | 50 | 0.48 | 2 | 125 | 175 |
V3P6 | 3 | 60 | 60 | 0.48 | 3 | 125 | 150 |
V3P6L | 3 | 60 | 80 | 0.44 | 3 | 125 | 150 |
V3PM6 | 3 | 60 | 80 | 0.47 | 3 | 125 | 175 |
V2PM10L | 2 | 100 | 50 | 0.58 | 2 | 125 | 175 |
V3PM10 | 3 | 100 | 80 | 0.58 | 3 | 125 | 175 |
V2PM12L | 2 | 120 | 50 | 0.6 | 2 | 125 | 175 |
V3PM12 | 3 | 120 | 80 | 0.61 | 3 | 125 | 175 |
V2PM15L | 2 | 150 | 50 | 0.64 | 2 | 125 | 175 |
V3PM15 | 3 | 150 | 80 | 0.64 | 3 | 125 | 175 |
V2P22L | 2 | 200 | 50 | 0.68 | 2 | 125 | 175 |
V3P22 | 3 | 200 | 60 | 0.7 | 3 | 125 | 175 |
Samples and production quantities of the new TMBS rectifiers are available now, with lead times of eight weeks for larger orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.TM Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
https://twitter.com/vishayindust
https://www.facebook.com/VishayIntertechnology
###
TMBS is a registered trademark of Vishay Intertechnology.
Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/