Vishay Intertechnology Best in Class 30 V N-Channel MOSFET Delivers High Power Density and Efficiency for Isolated and Non-Isolated Topologies
Devices Offers RDS(ON) Down to 0.95 mΩ and Improved FOM of 29.8 mΩ *nC in PowerPAK® 1212‑8S Package

Products mentioned:
SiSS52DNMedia Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
This release in:
- English
- Deutsch
MALVERN, Pa. — May 24, 2021 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a versatile new 30 V n-channel TrenchFET® Gen V power MOSFET that delivers increased power density and efficiency for both isolated and non-isolated topologies. Offered in the 3.3 mm by 3.3 mm thermally enhanced PowerPAK® 1212-8S package, the Vishay Siliconix SiSS52DN features best in class on-resistance of 0.95 mΩ at 10 V, a 5 % improvement over the previous generation product. In addition, the device delivers on-resistance of 1.5 mΩ at 4.5 V, while its 29.8 mΩ*nC on-resistance times gate charge at 4.5 V — a critical figure of merit (FOM) for MOSFETs used in switching applications — is one of the lowest on the market.
The SiSS52DN’s FOM represents a 29 % improvement over previous-generation devices, which translates into reduced conduction and switching losses to save energy in power conversion applications.
The SiSS52DN is ideal for low side switching for synchronous rectification, synchronous buck converters, DC/DC converters, switch tank topologies, OR-ring FETs, and load switches for power supplies in servers and telecom and RF equipment. By delivering high performance in isolated and non-isolated topologies, the MOSFET simplifies part selection for designers working with both.
The device is 100 % RG- and UIS-tested, RoHS-compliant, and halogen-free.
Samples and production quantities of the SiSS52DN are available now. For details and lead time information please contact your nearest Vishay sales office.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
https://www.facebook.com/VishayIntertechnology
###
The DNA of tech™ is a trademark of Vishay Intertechnology. TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated.
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
This release in:
- English
- Deutsch