News » 2023 Releases » Vishay Intertechnology Signs Agreement With Immersion to Bundle Haptic Te ...

Vishay Intertechnology Signs Agreement With Immersion to Bundle Haptic Technology Licenses With IHPT Series Actuators

2023-Immersion-VSH
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
MALVERN, Pa. — Aug. 21, 2023 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it is releasing a new series of IHPT solenoid-based haptic actuators that are bundled with patent licenses for Immersion Corporation’s (NASDAQ: IMMR) haptic technology. The bundled offering streamlines the design-in process for these devices and eliminates the need for a separate license to implement haptic effects.

Vishay’s IHPT series haptic actuators utilize compact and cost-effective solenoid technology to provide high force level HD effects with a drive voltage between 8 V and 16 V. The first device in the series — the IHPT1411 — provides a force level up to 120 N. Dimensions for the IHPT1411 are 35 mm by 35 mm by 16 mm. Additional devices offering a variety of force levels and sizes will be available later in 2023 to cover a wide range of automotive and commercial applications.

Since Vishay’s IHPT actuators operate off commonly available 12 V systems with IC driving circuits, they lower the cost of implementing haptic experiences in a wide range of end products. Applications for the IHPT series include LCD touchscreens, touch panels, buttons, rotary knobs, joysticks, and other human machine interfaces (HMI).

Vishay provides basic guidelines on how to mount and drive the IHPT actuators to create a basic suite of haptic experiences that the user can build on for their specific application. Learn more at www.vishay.com/doc?34604.

Due to licensing restrictions, IHPT haptic actuators are not available for certain applications, including gaming. For more information on use restrictions, please visit www.vishay.com/doc?34602.

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

facebook https://www.facebook.com/VishayIntertechnology

###

The DNA of tech® is a trademark of Vishay Intertechnology.
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
Resources Design Tools Document Library Engineer's Toolbox Infographics My Vishay New Products Reference Designs Technical Support Videos

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.®


Contact Us |
Where to Buy
  • Find a Distributor
  • Find a Sales Representative
| Request Sample | Privacy Center | Do Not Sell or Share My Personal Information | Terms and Conditions | Information Security | Terms of Use | Legal Notice |

CONNECT WITH US

Copyright ©2026 Vishay Intertechnology, Inc.

ECIA Member