Vishay Intertechnology 2 A and 3 A FRED Pt® Ultrafast Rectifiers in SlimSMAW Package Increase Reliability and Improve AOI
100 V and 200 V Devices are Footprint-Compatible With SOD-128 Package, Offer Larger Lead Widths Than SlimSMA
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Feb. 12, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its offering of Fred Pt® Ultrafast recovery rectifiers with eight new 100 V and 200 V devices in the eSMP® series SlimSMAW (DO-221AD) package with a low 0.9 mm profile. Footprint-compatible with the common SOD-128, the Vishay Semiconductors diodes feature larger lead widths than devices in the SlimSMA for increased reliability.
The 2 A and 3 A rectifiers released today offer high current density, while their wide leads provide stronger adhesion to the PCB and improve automated optical inspection (AOI) in automotive systems. FRED Pt® Ultrafast technology enables ultrafast recovery times down to 16 ns at TJ = 25 °C, reduced Qrr to 20 nC, and soft recovery features over the entire working temperature range of ‑55 °C to +175 °C.
Available in AEC-Q101 qualified versions, the rectifiers feature low forward voltage drop down to 0.69 V, which reduces power losses and improves efficiency in high frequency inverters, DC/DC converters, freewheeling diodes, and power factor correction in automotive engine control units (ECU), anti-lock braking systems (ABS), and HID and LED lighting, and telecom and industrial power supplies.
The devices offer an MSL moisture sensitivity level of 1, per J-STD-020, LF maximum peak of +260 °C. RoHS-compliant and halogen-free, the diodes are ideal for automated placement.
Device Specification Table:
Part # | IF(AV) (A) | VBR (V) | Typ. VF at IF at Tj | trr1 (ns) | Qrr2 (nC) | AEC-Q101 | |
(V) | (A) | ||||||
2 | 100 | 0.69 | 2 | 15 | 20 | N | |
2 | 100 | 0.69 | 2 | 15 | 20 | Y | |
2 | 200 | 0.69 | 2 | 15 | 20 | N | |
2 | 200 | 0.69 | 2 | 15 | 20 | Y | |
3 | 100 | 0.71 | 3 | 16 | 23 | N | |
3 | 100 | 0.71 | 3 | 16 | 23 | Y | |
3 | 200 | 0.71 | 3 | 16 | 23 | N | |
3 | 200 | 0.71 | 3 | 16 | 23 | Y |
1TJ = 25 °C, IF = 1 A, dIF/dt = 100 A/µ, VR = 30 V
2TJ = 125 °C, IF = rated current, dIF/dt = 200 A/µs, VR = 100 V
Samples and production quantities of the new Ultrafast rectifiers are available now, with lead times of 14 weeks for large orders.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
https://www.facebook.com/VishayIntertechnology
###
FRED Pt is a registered trademark of Vishay Intertechnology
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/